Post Go back to editing

adcmp601 spice simulation

Hi. I'm newbie of circuit simulation.

I need a threshold detection circuit using adcmp601.

I design circuit like this. the summing amp sum three signals, and adcmp601 detects the summed signal over threshold.

So I downloaded ad8000 and adcmp601 spice model from analog device website. I can simulate ad8000. But the problem is adcmp601.

I got this error from session log.

I googled this error and I can find adcmp601 is for hspice and I think the errors come from syntax difference.

From model editor there are these syntax.

e0 18 0 17 0 4 max=0.3 min=-0.3

e1 20 0 19 0 1 max=0.3 min=-0.3

Is there anyone know how to simulate hspice model in orcad?

I also tried another simulator ADsimPE provided by analog device, but same result. This is the result from ADsimPE.

Thank in advance!

Dongjin

Parents Reply Children
No Data