ADA4895-1 output noise

I would like a sanity check on my noise calculation and the actual result and any other comments.

Two ADA4895-1 op-amps in series each with a non-inverting gain of 10x. Rf = 226 ohms. Rg = 25.1 ohms, Rs = 51 ohms.

They are followed by an AD8021 with a non-inverting gain of 1. That is followed by a single pole R-C filter with 249 ohms and 18pF into an AD9240 ADC. The R-C filter frequency should be 35MHz. 55MHz was used due to the 1.57 single pole factor.

     From the ADA4895-1 datasheet:

236 MHz, −3 dB bandwidth (G = +10)

voltage noise is 1nV / SQRT(Hz)

current noise is 1.6pA / SQRT(Hz)

With the input grounded what is the predicted amplifier output noise into the AD9240? For my first approximation I ignored the AD8021 and assumed the first stage ADA4895-1 would dominate.

Scott

Parents
  • Harry,

    Sorry, I didn't expect someone to do the full calculation. Was just looking for a sanity check.

    The actual results measured using the AD9240 are below. The application is sensitive to peak voltages so that is shown along with the RMS conversion using 6.6, 99.9%. AD9240 is at the left of the list.

    No buffer, AD9240 inputs shorted = 1.53mV pk-pk = 231uV RMS

    AD8021 buffer = 2.14mV pk-pk = 324uV RMS

    AD8021 buffer + AD8021 at x2.5, x5 and x10 all = 2.75mV pk-pk = 416uV RMS

    AD8021 buffer + x5 AD8021 + x10 ADA4895-1 = 4.58mV pk-pk = 694uV RMS

    AD8021 buffer + x10 AD8021 + x10 ADA4895-1 = 9.16mV pk-pk = 1.38mV RMS

    The x10 noise from an AD8021 is the same as the noise from a 10x ADA4895-1 as the only amp.

    The result is that gains over 50x do not help as the noise from 50x to 100x doubled.

    Scott

Reply
  • Harry,

    Sorry, I didn't expect someone to do the full calculation. Was just looking for a sanity check.

    The actual results measured using the AD9240 are below. The application is sensitive to peak voltages so that is shown along with the RMS conversion using 6.6, 99.9%. AD9240 is at the left of the list.

    No buffer, AD9240 inputs shorted = 1.53mV pk-pk = 231uV RMS

    AD8021 buffer = 2.14mV pk-pk = 324uV RMS

    AD8021 buffer + AD8021 at x2.5, x5 and x10 all = 2.75mV pk-pk = 416uV RMS

    AD8021 buffer + x5 AD8021 + x10 ADA4895-1 = 4.58mV pk-pk = 694uV RMS

    AD8021 buffer + x10 AD8021 + x10 ADA4895-1 = 9.16mV pk-pk = 1.38mV RMS

    The x10 noise from an AD8021 is the same as the noise from a 10x ADA4895-1 as the only amp.

    The result is that gains over 50x do not help as the noise from 50x to 100x doubled.

    Scott

Children
No Data