Specification details for AD8099


Hi,

We have data for +/-5V and + 5V operating condition .

Do you have details of the Spec details  when used at +12 V .

Thanking you

With best regards and wishes

Parents
  • Hi,

    The DISABLE pin can be configured depending on the supply voltage you apply. When the DISABLE pin is supplied 2.6V below the positive supply(low), it activates the high impedance state of the part. Please see table below for convenience.

     

    Supply Voltage +10V +12V
    Disable 0 to + 7.4 0 to + 9.4
    Enable open open
    Low Input Bias 9.3 to 10 11.3 to 10

    I hope this helps.

    Regards,

    Roel

Reply
  • Hi,

    The DISABLE pin can be configured depending on the supply voltage you apply. When the DISABLE pin is supplied 2.6V below the positive supply(low), it activates the high impedance state of the part. Please see table below for convenience.

     

    Supply Voltage +10V +12V
    Disable 0 to + 7.4 0 to + 9.4
    Enable open open
    Low Input Bias 9.3 to 10 11.3 to 10

    I hope this helps.

    Regards,

    Roel

Children
No Data