Specification details for AD8099


Hi,

We have data for +/-5V and + 5V operating condition .

Do you have details of the Spec details  when used at +12 V .

Thanking you

With best regards and wishes

Parents
  • Hi wallman,

    We have only characterized AD8099 for +5 and +/-5V supplies. All the characterization data that we have is already in the datasheet. The +5V supply table should give you an idea on the performance of part at a +12V supply.

    Yes, you can connect the controller directly to the DISABLE pin as long as you set the proper supply voltage level (please see Table 5 of the datasheet). You can have an option to disable or enable the part or reduce the input bias current.

    Let us know if you need anything else.

    Regards,

    Roel

Reply
  • Hi wallman,

    We have only characterized AD8099 for +5 and +/-5V supplies. All the characterization data that we have is already in the datasheet. The +5V supply table should give you an idea on the performance of part at a +12V supply.

    Yes, you can connect the controller directly to the DISABLE pin as long as you set the proper supply voltage level (please see Table 5 of the datasheet). You can have an option to disable or enable the part or reduce the input bias current.

    Let us know if you need anything else.

    Regards,

    Roel

Children
No Data