Specification details for AD8099


Hi,

We have data for +/-5V and + 5V operating condition .

Do you have details of the Spec details  when used at +12 V .

Thanking you

With best regards and wishes

  • 0
    •  Analog Employees 
    on Jun 12, 2016 4:57 PM

    Hi,

         I am moving this thread to the amplifier community. Somebody will help you with your inquiry.

    Regards,

    Jonathan

  • Hi ,

    I am not able to post question in Amplifier area .

    I have another question with regards to Enable / Disable function on AD8099.

    Can we connect to controllers output open collector so that we can enable AD8099 for normal operation.

    How to use the Enable / Disable with controller, is this  possible .

    Please let me know there is a reference circuit using Disable function .

    [Enable Pin Leakage Current] Condition is DISABLE = 5 V in this condition the device will be Low Input Bias Current

    Thanking you

    With regards and wishes

  • Hi wallman,

    I contacted the product owner regarding this. I will get back to you once i have the information.

    Best regards,

    Roel

  • Hi  Roel,

    Is it fine to use a Open collector and switch of the Transistor ,please let me know with regards to leakage current when DISABLE pin is connected to Hi-Z .

    Please let me know the internal circuit connection ,is it a resistor divider circuit used to fix the voltage .

    Thanking you

    With best regards and wishes

  • Hi wallman,

    We have only characterized AD8099 for +5 and +/-5V supplies. All the characterization data that we have is already in the datasheet. The +5V supply table should give you an idea on the performance of part at a +12V supply.

    Yes, you can connect the controller directly to the DISABLE pin as long as you set the proper supply voltage level (please see Table 5 of the datasheet). You can have an option to disable or enable the part or reduce the input bias current.

    Let us know if you need anything else.

    Regards,

    Roel