I have a question about AD8676.http://www.analog.com/media/en/technical-documentation/data-sheets/AD8676.pdf#1, Does AD8676 will occur "phase reversal" when the input voltage exceed input common mode range? Some data sheet say "No phase reversal ", But this datasheet is not mentined.
Just in case, We are using this device under the following condition:G=1(Non-Inverting),Power supply=±5V(input common range =±3)
#2,Is it possible to use SPICE simulation to see "phase reversal"?
]
Best regards,Tarzan
Hi Harry,
Sorry that I couldn't respond this quickly.
Does that mean there is a possibility that the phase reverse like the following picture will occur?
http://www.analog.com/media/en/training-seminars/design-handbooks/Op-Amp-Applications/Section7.pdf
Best regards,
Tarzan
Thanks for your reply.
I was a bit worried about phase reverse behavior(like the picture), but glad to know that there is nothing like that.
I will implement something not to exceed IVR.
Thanks ,