Hi,
I would like to know the common mode voltage range of ADA4522-2. I am using this as a buffer. The supply voltage to the Op-Amp is ±5 V and my input would be near to 5V( assume 4.9V). What can be my possible output value.?
Thanks in advance.
Hi Emman,
Thanks for the reply. It did provide me good information.
I was looking for a dual op-amp with ±5V. So i feel we cannot use AD4528. Instead i have found AD8572 as a better option for the current scenario.
i am targeting for an offset of less than 10uV, so that no matter the temperature changes i would still be getting a stable output.
As of now I dont need negative voltage, because my output will be always positive.
I was just following the legacy circuit.
Since you asked me this, I would like to know what is the pros and cons of selecting single and dual Op-amps. Is it only depending on whether the application need positive and negative voltage??
What difference does it makes in a buffer circuit when I am using ±5V and +5V and ground as the supply voltage??
Regards,
Ashok