There is a small error in ADA4897 spice model, where node 106 (PD) should be DISABLE bar, i.e., when 106 pulled to -VS + 0.7 V, AD4897 will be put into disable mode.
There is a small error in ADA4897 spice model, where node 106 (PD) should be DISABLE bar, i.e., when 106 pulled to -VS + 0.7 V, AD4897 will be put into disable mode.
We will see on what we can do on this suggestion. Thanks.
I mean that this pin should be named as DISABLE#, rather that PD. When we build a symbol using A, we usually mean that A is a HIGH valid signal, for example PD means this chip is Power Down when PD is HIGH. For A#, we mean that A is a LOW valid signal, DISABLE# means that this chip is disabled when this pin is LOW.