AD8421 output oscillation with no input signal

I have a pcb with the following circuit. 

The inputs (left side) are small DC voltages, within ~100mV of ground. They won't be DC in the final application, but for debugging that's what they are. No gain resistors are used. There are decoupling caps on the +/- 15V power supply (0.1uF ceramic 0402 close to pins, 10uF tantalum 1206 next, then 1mF electrolytic ~3cm from pins). It's a lab power supply, very clean. 

The output signal is a very clean oscillation ~1V peak to peak, ~6 MHz. Shown below are the inputs (traces 3 and 4, purple and pink respectively), and the output in green.  

When I add a 10nF cap in parallel with the 1kOhm output resistor, R5, I get the trace below, with a ~2MHz frequency but similar amplitude.

I added a 10uF ceramic capacitor in parallel with R5, and the oscillations were either small enough that I couldn't see them on the scope any more or they were gone entirely. I may be able leave the output cap in my final circuit, but I would be much more comfortable with doing so if I understood where this problem was coming from. 

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:48 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:48 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data