Post Go back to editing

Can the ADA4922-1 be operated from a single 5 V supply?

I'm looking for a single-ended to differential amplifier which can be powered by a single 5 V supply.  I.E. Vs+ = 5.0 V, Vs- = 0V.

The ADA4922-1 fits the bill otherwise, and we already use it in some products.

The datasheet advises a supply range of 5 V to 26 V, but unlike other Analog datasheets (AD8137, etc.), never specifies or even mentions operation from a single supply. 

It is not clear to me if the datasheet specifications apply only to bipolar supplies, effectively meaning +-5 V to +-26 V.