Post Go back to editing

Operating range of the AD790

I have read the AD790 datasheet.
It is a question about the operating range of the AD790.
The AD790 data sheet says "Dual? 15 V Supply Operation".
And the AD 790 data sheet says "ABSOLUTE MAXIMUM RATINGS Supply Voltage ± 18 V".
The AD790 has a GROUND terminal.

In case When saying the data sheet is ± 18 V, is it relative to the GROUND terminal?

Best regards

Parents
  • Hi Mochi,

    The recommended supply range for the AD790 is +/-15V which means +15V to the +Vs pin and -15V to the -Vs with respect to the AD790's ground pin.

    The absolute maximum ratings is also referred to the device ground pin but operating outside this range could cause permanent damage to the part.

    Best regards,

    Rainier

Reply
  • Hi Mochi,

    The recommended supply range for the AD790 is +/-15V which means +15V to the +Vs pin and -15V to the -Vs with respect to the AD790's ground pin.

    The absolute maximum ratings is also referred to the device ground pin but operating outside this range could cause permanent damage to the part.

    Best regards,

    Rainier

Children
No Data