ADA4610-1 Maximum Supply Voltage.

The device's datasheets specify a maximum supply voltage of +/- 18V.

Does this device have to supply a positive voltage?

My design is a structure that can only supply 24V of voltage.

I want to supply V +: 24V, V-: 0V.

Is there any problem with performance even if it works as above?

Parents
  • 0
    •  Analog Employees 
    on Mar 25, 2018 6:25 PM

    Hello, 

    Yes, the ADA4610 should still work with a 24V single supply. In general, operational amplifiers can be used in a single supply configuration for as long as the difference between the supplies is kept within the specification. You should just take care to keep your inputs within the supplies. Also, keep in mind that the output will only be able to swing within those supplies. 

    May I ask what your application is? 

    Thanks, 

    Kris

Reply
  • 0
    •  Analog Employees 
    on Mar 25, 2018 6:25 PM

    Hello, 

    Yes, the ADA4610 should still work with a 24V single supply. In general, operational amplifiers can be used in a single supply configuration for as long as the difference between the supplies is kept within the specification. You should just take care to keep your inputs within the supplies. Also, keep in mind that the output will only be able to swing within those supplies. 

    May I ask what your application is? 

    Thanks, 

    Kris

Children
No Data