ADA4084 Settling Time

Hi,

-Do you know what does the 0.1% means in the test conditions of settling time ? (see below)

Settling Time : ts : AV = 10, VIN = 10 V p-p, 0.1%        typ:4µs.

- I did not understand figure 30, 61,92 of settling time.

For Figure 92, Vsy=+/-15V, Input switch to -5V to +5V. Output finishes at 0V from which value ? It's not an Av of 10 ?

BR,

Mathieu