Hi,
I am testing the LT1711 and connected the following load circuit to its outputs:
The device is powered by +5V and -5V.
With the above load, Ioh=10mA.
OUT+ and OUT- toggle between 0.15V to 4.7V.
There is no hysteresis in this circuit.
When measuring Tr and Tf:
OUT+ : Tf > Tr by ~1ns (Tr=~2ns; Tf=~3ns)
OUT- : Tr very similar to Tf, and equal ~4ns.
My questions:
1. I expect Tr for OUT+ to equal Tf for OUT- (and Tf for OUT+ to equal Tr for OUT-) since both OUT+ and OUT- go into a differential input stage.
Why is the un-symmetry here?
2. Tr and Tf for OUT- are higher than the ones for OUT+.
both output stages should be symmetrical (the load is symmetrical).
Why is this un-symmetry?
Thank you
Gil