Post Go back to editing

Comparator stability - AD8561 versus LT1711

hello,

I've been using the ad8561 in the following circuit:

IN- connected to OUT- via few resistors (hystersis of few tens of mV) around 0V.

IN+ gets a sine wave signal with frequencies as low as 100Hz. When crossing the 0V point, the output toggles.

There are no oscillations on the output (due to low SR of the sine wave input).

Since the ad8561 is not a rail-to-rail input device, I've taken the LT1711 and I use it similarly (see below).

Vin is the sine wave signal. I've used hysteresis resistors of 50ohm/12.4K (20mV) and even 300ohm/10K (134mV).

On the LT1711 Ioh=10mA.

Both comparators are powered from +5V and -5V.

My problem: The ad8561 outputs are stable in Vin sine wave frequencies as low as 100Hz (and even lower).

With the LT1711 the outputs oscillate when Vin is 90KHz and lower.

Why?

Thank you

Gil

Parents
  • Hi gil_he:

    Do the oscillations occur when the inputs are near zero cross?   That could actually be a noise problem rather than an oscillation, and might be fixed with a little more hysteresis.

    The LT1711 is quite a bit faster than AD8561.  The LT1713 is more similar to the AD8561.  If you didn't want the extra speed of the LT1711, then you could use the LT1713 instead.   The higher bandwidth of the LT1711 will give you more total input noise.

  • Hi Glen,

    I am testing now the LT1713. Same setup.

    The oscillations are much "better".

    With an input signal of 10Hz, feedback cap of 4.7pF, hsyteresis of 40-100mV (few scenarios), Iout of 10mA (also tested with 7mA):

    Output /Q is stable. No oscillations.

    However, output Q starts oscillating (at the beginning of the change) at frequencies of 5KHz and lower.

    Why is this?

    thank you

    Gil

Reply
  • Hi Glen,

    I am testing now the LT1713. Same setup.

    The oscillations are much "better".

    With an input signal of 10Hz, feedback cap of 4.7pF, hsyteresis of 40-100mV (few scenarios), Iout of 10mA (also tested with 7mA):

    Output /Q is stable. No oscillations.

    However, output Q starts oscillating (at the beginning of the change) at frequencies of 5KHz and lower.

    Why is this?

    thank you

    Gil

Children
No Data