Post Go back to editing

ADCMP580 Latch Enable/Disable

Hey Guys

I'm trying to make sense of the ADCMP580 data sheet regarding the latch function. In the pin description on Page 7, Table 4, it says that the LEB pin needs to be low and LE = high in order to use the ADCMP280 in comparator mode. But on Page 12 "USING/DISABLING THE LATCH FEATURE" it says that for disabling the latch feature, the LEB and LE pins need to be the other way around (which would make sense to me since the pins are labeled as "Latch Enable"). But which one is true? And whats the function of the VTT pin exactly? An equivalent input schematic of this LEB/LE/VTT thing would be very helpful.

Thanks and regards
Fabian