Hi,
I would like to use LT6106.
So, I have a question. Please help me.
Question:
I have a question about datasheet p.3.
Below is the electrical characteristic about Vout (High).
When Vsense = 120 mV, there is 1.2 V max (1.4 V at the whole temperature) ,
but there is a doubt about the specification at this time.
I think that Vout is calculated by the following formula.
Vout = Vsense * Gain
(Gain = Rout / Rin)
At this time, because Vsense = 120 mV, Rin = 100 Ω, Rout = 10 kΩ, Gain = 100 in the specification, I think that Vout will be 12 V.
Is this a mistake in the datasheet?
If erroneous, please tell me the official range of Vout Swing.
Best Regards,
Naohisa
Title change
[edited by: naohisa at 3:43 AM (GMT 0) on 13 Feb 2019]