Post Go back to editing

(ADA4096-2)Can we input 30V when the power supply is 0V?

Hi !

I have a question about ADA4096-2.

At datasheet, it says absolute maximum is "(-V)-32V < Vin <(+V)+32".

Does this mean if -V = +V = 0V, can we input ±32V to Input pins?


Best regards

Kawa

Parents Reply
  • Hi !

    Thank you for your reply.

    I understand what you said.

    What I want to make sure is, if some voltage input to the device even if the power is off, would it broke the device.

    As you said, I understood that setting V+ = V-  = 0V, would be fine but you would not be able to bias the internal transistors.

    If the device don't output anything when the power is off, it is ok.

    Do you mean if we input 30V when power is 0V, would it broke the device?

    Best regards

    Kawa

Children