Post Go back to editing

(ADA4096-2)Can we input 30V when the power supply is 0V?

Hi !

I have a question about ADA4096-2.

At datasheet, it says absolute maximum is "(-V)-32V < Vin <(+V)+32".

Does this mean if -V = +V = 0V, can we input ±32V to Input pins?


Best regards

Kawa

Parents Reply
  • Hi,

    It is always recommended to operate on specified conditions. Operating at the abs max condition tells that if you exceed that value we would not be able to guarantee that the part will work beyond that.

    Also, setting V+ = V-  = 0V, would be fine but you would not be able to bias the internal transistors.

Children