Hi,
We do have a catheter cable length of 2.4 meter , trying to understand if the amplifier ADA4950-1 will be able to drive the same or not?
We have set this for a gain of 2. The input level from the FPGA is driven as 2.4V p-p, output of the ADA4950-1 is seen as 4.8V p-p.
There is a change in rise time of the signal (20Mhz burst clocks) that are transmitted via cable!
Can you share the output capacitance driving capacity for the part ADA4950-1.