Post Go back to editing

ADA2200 Program filter setting and Output waveform calculation

Hi,

There are two questions about use ADA2200.

1. Regarding to the ADA2200 Program filter function, Could you please help to provide some reference data for the Program filter setting. The datasheet doesn't tell too much about it.

2. Regarding to the output waveform, the datasheet says -

In the default configuration, there are eight output sample periods during each RCLK cycle. There are four updated output samples while the RCLK signal is high. While RCLK is low, the fourth updated sample is held constant for four additional output sample periods.  (Page 13, Mixer section)

Does it means only half cycle waveform will be present (As below figure) ??  How to calculate the input waveform value?

Hear from you soon and thanks!

Parents
  • Hi Brent,

    We have a tutorial, MT-234, on using the programmable filter of the ADA2200 at this link. I hope that will answer your first question.

    Regarding your second question...the ADA2200 mixing function produces a sampled output that is in between a 1/2 wave rectification and a full-wave rectification. To measure the input waveform value you can do one of the following:

         - Low pass filter the output and measure value

         - Calculate the cycle mean. This is done by sampling 8 consecutive output values (5 unique values+3 hold values) and taking the average value.

    Regards,

    Brian

Reply
  • Hi Brent,

    We have a tutorial, MT-234, on using the programmable filter of the ADA2200 at this link. I hope that will answer your first question.

    Regarding your second question...the ADA2200 mixing function produces a sampled output that is in between a 1/2 wave rectification and a full-wave rectification. To measure the input waveform value you can do one of the following:

         - Low pass filter the output and measure value

         - Calculate the cycle mean. This is done by sampling 8 consecutive output values (5 unique values+3 hold values) and taking the average value.

    Regards,

    Brian

Children
No Data