Hello,
When performing a noise simulation in LTSpice, the results showed a noise level of 2.0 mV/√Hz at 100 mHz, decreasing toward 0.0 mV/√Hz as the frequency approached 1 kHz. Could you please provide your perspective on this? Specifically, is the simulation correct, is this a characteristic of the device itself, or is there an issue with the model data?
Circuit diagram created by the customer
ADA4941_sim.asc
The customer is creating the circuit schematic in accordance with AN-1495. The specific details are being handled by the customer.
How to create model data for the ADA4941.
1. Download the .cir file from the "ADA4941 SPICE Macro MODEL" section under "Tools & Simulations" on the ADA4941 webpage.
2. Open the LTspice .asc file provided by the customer; then, go to File > Open and select the corresponding .cir file—which should be located in the same folder as the .asc file—by choosing "Netlists (*.cir, *.net, *.sp)" as the file type.
3. Place the cursor on a line in the netlist that begins with ".SUBCKT," then select "Create Symbol" from the right-click context menu.
4. Import the generated .assy data and start the simulation.
5. The curve in the upper left shows the result obtained by applying a probe to OutP.
The customer comment
I downloaded the ADA4941 SPICE Macro Model from the webpage, built the circuit according to the APPLICATION NOTE (AN-1495), and performed a simulation using LTspice.
After performing a transient analysis and confirming that the differential converter was functioning correctly, a noise analysis revealed noise levels higher than expected.
(Noise is occurring in the mV range.)
Given that this noise level deviates significantly from the device's performance, I suspect there may be a problem with the SPICE Macro Model.
I have attached the circuit diagram (.asc file). Please verify that there are no errors in the low-frequency noise (1/f noise, etc.) settings within the model.
As the customer suggests, could this be due to device performance, or is there a possibility of an error in the simulation methodology or the circuit configuration?