Post Go back to editing

Frequency doubler shown in data sheet 14 is not working at all , is there any corrections to the datasheet

Thread Summary

The user encountered no output when using the same schematics as the datasheet for a frequency doubler. The final answer identified that the R2 resistor should be connected directly across X1 and X2, not between X2 and Y2 as shown in the user's schematic. The user confirmed that the LTSpice simulation worked but not the breadboard or proto board implementation.
AI Generated Content
Category: Hardware
Product Number: AD734

  

Used the same schematics as the datasheet with since wave input , no output