Hi Analog Team,
I like to have a second opinion on the impelentation of an ADC driver we need to build in.
In a current design, we are using an VGA (AD8336ACPZ-R7) that is directly connected to an ADC (LT2249) input.
Well, lessons learned, we are unable to to achieve the full-input swing of 1 Vpp, due to a high output impedance of the VGA.
That means, we definitely need to integrate an FDA as ADC Driver.
Before finally changing the layout, I would like to get some thoughts and confirmation from your point of perspektive.
The bandwith for the system should be approx. >=10 MHz.
We have +-12V Supply Rail (powering the VGA), a 3.3V rail (ADC) and a 5V source.
As far as I see, FDAs are much more available for 5V-Rails.
Currently I would like to move forward with the AD8138.
Below are two design in proposals. Should I better use the AC coupling with or w/o termination?


Unfortunately, it's not possible to simulate the VGA Amp in LT Spice with transient analysis, at least I can't succeed to get it running.

If you have further recommendations, please let me know.
Thanks a lot,
Christian