ADA4945-1
Recommended for New Designs
The ADA4945-1 is a low-noise, low-distortion, fully differential amplifier with two selectable power modes. The device operates over a broad power supply...
Datasheet
ADA4945-1 on Analog.com
Hi Team,
I'm planning to use ADA4945-1ACPZ-R2 as input amplifier for my ADC AD7768.
My requirement output range of the Amplifier is +/-4V as it our requirement of the ADC.
For the above input voltage range can i use the AVDD1 - 5V, AVDD2 - 5V, IOVDD - 1.8V for ADC with amplifier supply voltages +5V for Vs+ & -5V for Vs-.
Also want should be gain should i provide to the amplifier for getting +/-4V output range. I requirement is that input will be singled ended signals and output needs to be differential.
Please provide a suggestion for my design.
Regards,
Abhishek
Hello AbhishekManoj,
I will proceed to close this query as this was a duplicate of (+) Design Inquiry - Q&A - Differential Amplifiers and ADC Drivers - EngineerZone
Regards,
Paul
Hello AbhishekManoj,
I will proceed to close this query as this was a duplicate of (+) Design Inquiry - Q&A - Differential Amplifiers and ADC Drivers - EngineerZone
Regards,
Paul