Post Go back to editing

LTC6409 Vocm not functioning as expected

Category: Hardware
Product Number: LTC6409

Hi,

I'm running a LTSpice simualtion with the LTC6409. The simulation is running as expected with the exception of the following Vocm value. When the value of Vocm is set from 1V to 1.25V, the output of the LTC6409 deviates significantly from expected / Vocm=1V.

LTC6409 is functioning as expected with Vocm = 1V.

LTC6409 is not functioning as expected:

What's going on? I don't see this phenomenon documented in the datasheet.

Thanks,

Ethan