Post Go back to editing

On impedance matching when a single-ended signal from a preamplifier is fed into a post single-ended-to-differential amplifier to be converted into a differential signal

Category: Hardware
Product Number: ADA4932-2

Hi, I have encountered the following problem in designing a single-ended to differential circuit, my signal source is the output signal of an amplifier, which is connected to the back-end single-ended to differential circuit, at this time, is the impedance of my signal source based on the output impedance of the preamplifier? As well as in the back-end differential amplifier, in order to achieve impedance matching, usually connected to a calculated to ground resistance R7, to 50 Ω source as an example, the presence of this to ground resistance will make my input signal is attenuated, this attenuation will affect the signal-to-noise ratio of the signal? Is there an alternative to this process to ensure that my single-ended differential input signal is not attenuated?

The first one shows the first stage amplifier, the second one shows the single-ended to differential amplifier

    

Parents Reply
  • Yes. I'm just confused about the resistor located at R7, in the chip manual he is there for impedance matching, but it affects the gain, there is confusion about this place.According to you, since the impedance of the front-end op-amp output is very small, then R7 should not be needed here, right? If it's not needed, the differential input impedance will be large, and will this process affect the signal?

Children
No Data