LTC6362
Last Time Buy
The LTC6362 is a low power, low noise differential op amp with rail-to-rail input and output swing that has been optimized to drive low power SAR ADCs...
LTC6362 on Analog.com
Hi guys,
I am looking for an IC to replace LTC6362 since it is declared as "Last Time Buy".
Must haves:
- As similar as possible as LTC6362
- BW(-3dB) of at least 30MHz
- PSRR of minimum 30dB at 30MHz
I would be very grateful for 1-2 IC suggestions that come as close as possible to the specs.
Thanks,
Can
PS:
Currently, the utilized LTC6362 has to come down to 200mV at its outputs, as well as to about 100mV at the inputs.
The proposed alternatives should also be able to do this.