In order to measure the current flowing through the shunt resistor, I want to use the LTC6362 peripheral circuit configured as below, but when the supply voltage is applied, the op-amp differential output is fixed at 3V. I don't know why.

LTC6362
Last Time Buy
The LTC6362 is a low power, low noise differential op amp with rail-to-rail input and output swing that has been optimized to drive low power SAR ADCs...
Datasheet
LTC6362 on Analog.com
In order to measure the current flowing through the shunt resistor, I want to use the LTC6362 peripheral circuit configured as below, but when the supply voltage is applied, the op-amp differential output is fixed at 3V. I don't know why.

Hello,
what input voltages are applied in that case?.
If no current is flowing, the differential input voltage is 0V, but still a common mode input voltage is applied. Is this inside the allowed input common mode voltage range? (It should range approximately from -1V to +4,xV in your case.)
If you exeed the allowed range, the chip may deliver strange results.
best regards
Achim
The shunt resistor is connected below fig, so I think the common mode voltage will be close to 0V.

Is there no problem with the circuit?
In addition, almost 0V is applied to C72 capacitor voltage
Hello,
if the shunt resistor is connected to GND, the input common mode voltage is OK.
Then I do not see any obvious problem in the schematic. If it does not work as expected I would first measure the voltages directly at each pin of the chip to check, if the pcb really is connected as the schematic shows (soldering problem or something similar).
best regards
Achim
It was confirmed that the 1.5V ref voltage sometimes shakes or rises to about 2.7V when LTC6362 is attached. In this regard, do we need to do anything additional to the Vocm pin?
If LTC6362 is not attached, 1.5V works well.
Hi dsazxc ,
Sorry for missing this thread. Can you try directly using a 1.5 V supply to the Vocm? If the LTC6362 works fine, I think there is a problem with the connection between the reference source and the LTC6362, which could cause the issue. Thank you.
Regards,
Gilbeys