Post Go back to editing

Input impedance matching

Thread Summary

The user is using the LTC6409 to level shift between an IQ demodulator requiring 3.5V common mode voltage and a vector modulator requiring 0.5V common mode voltage. The final answer suggests using 100 ohm resistors as a starting point for input matching, while the capacitor values should remain the same. The output is connected to the ADL5390, which requires a 0.5V common mode with a ±0.5V swing.
AI Generated Content
Category: Datasheet/Specs
Product Number: LTC6409

Hi. I am using LTC6409 to level shift an IQ demodulator that requires 3.5V common mode voltage with a vector modulator that requires 0.5V common mode voltage. From the components datasheet it can be seen that it uses some resistors and capacitors to differentially match the component with an IQ demodulator of 130Ω||2.5pF impedance. In my case the Demodulator has 200Ω||3pF differential impedance. The diagram has little explanation as to why it uses two 75ohm resistors or any of the capacitor values. What should i change to accommodate it for my own design. Thank you in advance.

Thread Notes

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.