hello:
i use an ada4940-1 to build a test circuit(as follows).i use the chip to convert a single-ended signal to differential.i found that there is a 1.6V output between out+ and out- when in+ is floating.i try to add R4(100K),and i found the output is 1.4V?
annd more,i use a desktop power source to provide the intput voltage,i found the current of the source is negative!
did i make a wrong use of the chip?