Post Go back to editing

Regarding output voltage fluctuation when switching gain

Category: Hardware
Product Number: AD8338

Hi,

I'm considering AD8338.

I am evaluating the AD8338 evaluation board.

When the gain of the AD8338 is changed, a phenomenon occurs in which the output of the AD8338 fluctuates more than the original output.
The same problem occurs with the default circuit of the AD8338 evaluation board (EVAL-AD8338) and with my prototype.
Is this a phenomenon specific to AD8338? Is there a solution?

【input signal】
・10kHz, 0.1Vp-p, single-ended input
・100Hz, 0.3Vp-p, Voffset = 0.4V, J3&J4=Open
→ Under these conditions, the output amplitude increases at the rise/fall of gain switching.

Best regards,

Yuya