Post Go back to editing

LTC6432 as 2x independent amps

Category: Datasheet/Specs
Product Number: LTC6432-15

Hello AD,

1. When using the LTC6432-15 as 2x independent amplifiers: If one of the amplifiers is to be disabled to save power, is an allowable way to achieve this to remove power from the corresponding output feed choke, and if so, would the expected power savings be close to 50%?

2. Is the PSRR of this part vs. frequency perhaps available?

3. Is a channel isolation spec over frequency perhaps available for this part?

Thread Notes