Post Go back to editing

After & before the ADA4817-2 reference voltage level shifting from 0 to another level automatically, because code is not loaded in board. Is there any way to keep it on zero reference level?

Category: Hardware
Product Number: ADA4817-2 DAC (Differential Input to single ended output)

1) After the ADA4817-2 reference level shifting to 1.6v from 0V automatically when board is in Power off condition(Code is not loaded).

2) this is at output before amplifier(ADA4817-2). Board is in Power ON condition but code is not loaded in board...  it shift voltage reference to 0.48V from 0V. It directly shifting here without running(loading) the code.