Post Go back to editing

What is AD8130 Impedance for PCB layout?

Category: Datasheet/Specs
Product Number: AD8130

Hi,

I am planning to use AD8130 as Receiver Amplifier in my design. What are the Input and Output impedance of AD8130. In datasheet it says 5 MΩ but I think 5 MΩ is a high value. I am drawing the layout of the PCB. Which value should I use for Impedance of the trace. Could you please help me?

Regards

Toprak

PCB traces for common designs are often set to 50+-10% Ohms. (55 Ohms nominally using common pre-preg and trace widths).   Input impedances don't matter, even digital circuits have high input impedances.  Output impedances are often in the 22-33 Ohm range which work well with 50 Ohm boards.

  • Hi,

    I believe that the question has already been answered so I am closing this thread. Thank you!

    Regards,
    Paul