Post Go back to editing

Relation between Vout and Vref in LT1999

Category: Hardware
Product Number: LT1999

Hello,

I have a question about the LT1999.

Is it possible that Vref > Vout in the following conditions?
(12 boards are created and one board is in the following state).

(1) V+ and V- are connected to a 1mΩ shunt resistor (4-terminal).
(2) A current of 0.3A flows so that V+ is higher.

On the block diagram, it is amplified based on Vref, but in the detection part of the previous stage, is it possible for some reason that a + value should be output but it swings to -?
Or is Vref > Vout due to some other factor?

I would appreciate it if you could reply.

Best Regards,

Knj