Post Go back to editing

MAX4198 use as MAX4199

Category: Hardware
Product Number: max4198

hello. 

I'm using MAX4199 to amplify output voltage.

However, I'm going to change MAX4199 to MAX4198 because of out of order.

My inquiry is below.

CAN MAX4198 amplifies output voltage like MAX4199 by configure peripheral curcuit?

If I use R147, 148 as 226Kohm then output gain can be change +1V/V to +10V/V?

Thank you.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.