Post Go back to editing

Several questions about ADCMP582 - High speed comparator

Thread Summary

The user is planning to use the ADCMP582 high-speed comparator and has questions about its input termination, VTT pin connection, and disabling the latch function. The final answer confirms that VTP and VTN can be used as termination ports, VTT should be connected to VCCO-2V, and provides a reference for connecting LE and LE-bar to disable the latch function. The user also asks about connecting ADCMP582 to MC100EP01, noting a potential mismatch in voltage levels between the two components.
AI Generated Content
Category: Hardware
Product Number: ADCMP582

Hello Guys,

We are planning to use high speed comparator chips. ADCMP582 seems to be suitable for our application. However, ADCMP582 datasheet leaves several uncertain questions to us. We have to confirm with ADI.

1. The input pins Vtp&Vtn, we can use them as input port Vp&Vn's termination port? Becasue which have intrinsic parallelly 50ohm to ground.

2. Vtt pin must connect to VCCO-2V?

3. How to connect LE and LE-bar to disable Latch function? The datasheet describes this about 580 and 581, but it doesn't have this part for 582.

We draw a roughly schematic of ADCMP582 according to our understand, can you help check it?

Edit Notes

"The datasheet describes this about 580 and 581, but it doesn't have this part for 582."
[edited by: coyoo at 7:28 AM (GMT -4) on 27 Mar 2023]
  • Hi Coyoo,

    Good day! Thank you for considering ADCMP582 for your application! 

    See below for each response:

    1. The input pins Vtp&Vtn, we can use them as input port Vp&Vn's termination port? Becasue which have intrinsic parallelly 50ohm to ground.
    -> Yes. That is exactly the purpose of VTP and VTN. If you connect them to GND, then VP and VN will be terminated to ground through the 50ohm resistor.

    2. Vtt pin must connect to VCCO-2V?
    -> Yes, connect VTT to VCCO-2V for ADCMP582

    3. How to connect LE and LE-bar to disable Latch function? The datasheet describes this about 580 and 581, but it doesn't have this part for 582.
    -> Please refer to figure 22 of the datasheet .

    To proceed in checking your schematic, may I know your target hysteresis and if you will enable latch function?
    Also, what will be your intended application?

    Thanks and Best Regards,
    Sham

  • Hi Sham,

    Thanks for u reply.

    Yes, we use this part to replace MAX9601, because we didn't get fine hysteresis. However, ADCMP582 seems can apply lower to 1 or 2mV controlling.

    As a driver, ADCMP582 in our case will be used to drive one OR gate chip (MC100EP01). So, I have a very serious question about how to connect between ADCMP582 and MC100EP01? We can't simply copy our previous design from MAX9601&mc100ep01. Because ADCMP582 introduce one "special" PECL, its Vol range is from VCCO-1.5 to VCCO-1.2 (1.8V~2.1V when VCCO is 3.3V).  However, the receiver, MC100EP01, only has its Vil range from 1.355V~1.675V. They are mismatched.

  • Apologies for missing your reply. Do you still need assistance in this one?

    Thanks,

    Mae

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.