AD630
Production
The AD630 is a high precision balanced modulator/demodulator
that combines a flexible commutating architecture with the
accuracy and temperature stability...
Datasheet
AD630 on Analog.com
AD5292
Production
The AD5291 and AD5292 are single-channel, 256-/1024-position digital potentiometers that combine industry leading variable resistor performance with nonvolatile...
Datasheet
AD5292 on Analog.com
Hi Dear,
Can I use a 20k digital potentiomenter (AD5292BRUZ-20) in the differential offset ajust and (other AD5292BRUZ-20) in the commum mode offset adjust?
Hi fbassan
Regarding the resistance value, we recommend using 10k pot. The pot is used to balance the collector current sources of the input transconductance stage and compensates for mismatches in transistor sizes, due to this the 10k value is OK.
May we ask the reason why you want to use a digital potentiometer? Is it something about the accuracy of resistance values, or you want to implement a system that can change the resistance values based on the resulting output voltages (feedback control system)? A simple trim pot is also applicable for this application since it is much simpler and cheaper.
Regards,
JE