Hi,
As below picture, it says that the differential input voltage of ADA4945-1 is ±1V.In the same way,the differential input voltage of ADA4940-1 is 1.2V.How to understand it? For ADA4945-1,if the differential input voltage is more than ±1V,Can this device work correctly? Is it not a rail to rail input amplifier? For ADA4940-1,the differential input voltage is only positive rail, without negative rail,why?
Thanks!