Post Go back to editing

AOP

Category: Hardware
Product Number: LT6233
Software Version: No

Hello,

I would like to find a equivalent with this component 'LT6233CS6#TRMPBF' because i have to order 5000 pieces. Do you know any components with the same footprint and the same function pins because I have already designed the PCB.

Thank for your helps

Regards

Parents
  • Hi ,

    I tried to look at the parametric search and found the following attached parts which have the same TSOT-23 6 pin package as the LT6233CS6.

    Hope this helps you one that is compatible / replacement.

    XLSX

    I've not looked to make sure the pins are identical or not. But, you can take a look and see if these parametrically satisfy the application or not first.

    Regards,

    Hooman

Reply
  • Hi ,

    I tried to look at the parametric search and found the following attached parts which have the same TSOT-23 6 pin package as the LT6233CS6.

    Hope this helps you one that is compatible / replacement.

    XLSX

    I've not looked to make sure the pins are identical or not. But, you can take a look and see if these parametrically satisfy the application or not first.

    Regards,

    Hooman

Children
  • Hi,

    Thank you, I'll look your XLSX if there is anything compatible. 

  • Hello, 

    I would like to know if this LT6233 is an instrumentation amplifier ? I can see in the DS :

    - Ultrasound Amplifiers
    - Low Noise, Low Power Signal Processing
    - Driving A/D Converters

    Because I pick up signals of order µV from a Hydrophone. 

    Thank for your helps

    Regards

  • Hi ,

    LT6233 is not an Instrumentation Amplifier. It's a Op Amp.

    Regarding the pick up you're seeing: Most of the pickups I've had to deal with are from the way the grounding and PCB layout are done. Sensitive input nodes are especially vulnerable and need to have to have good grounding and shielding.

    If you like, you can share more details and see if I (or others on the forum) can lend a hand to help resolve your interference pick up problem.

    Regards,

    Hooman

  • Most of the pickups I've had to deal with are from the way the grounding and PCB layout are done

    I'm not speaking for the moment of routing of the card. Can I use this AOP LT6233 to filter a signal coming from a Hydrophone (The Hydrophone already has an integrated preamp). I use this AOP as a high pass filter (the signal is about 1µV to 300µV). Can you answer this question first ?

    Thanks for your advice
     

  • Hi ,

    I recommend that you take a look at the Filter Wizard program link below to design your High Pass filter using LT6233:

    https://tools.analog.com/en/filterwizard/

    Let me know if you have any specific question regarding this design.

    Regards,

    Hooman

  • Hi Hooman,

    Your link I already tried but It can't give me a transient function. I can do it with LTspice and I have a offset with a small signal : 

      

    I have about 32 mV for an output voltage (for input voltage 1mV-1kHz). And an ADC don't like this offset.  

  • Hi ,

    Please attach your LTspice schematic (*.asc file) in here so that I / others can take a look and see if we can help resolve your offset issue.

    To attach a file, use Insert, Image/Video/File, go to the file location and click Upload, Ok.

    Regards,

    Hooman

  • Hi Hooman,

    Thank you for your helps, please see in this attached the simulation file. Just a point of precision, I add the second AOP to simulate a load with infinite impedance (in theory) and a link capacitance to remove the DC component. But nothing changes. 

     Draft1.asc

    Regards.

  • Hi ,

    Regarding the offset you're seeing from using LT6233 as a Sallen Key High Pass Filter:

    Most of that is due to the input bias current of LT6233 (3uA max) flowing through the 22.5kohm input resistor (R1).

    I've added a dummy current source to your schematic to allow you to change that current and see the output offset go away or increase (depending on the magnitude and direction of that current).

    Here is the simulation file:

    LT6233 Sallen Key Filter Offset EZ 7_11_22.asc

    To resolve this issue, you can do one or both of the following:

    1. Scale your R's lower and your C's higher (to maintain the same filter response) by the same factor (e.g. 22.5k ->2.25k and 1uF --> 10uF, etc.) to reduce the impact of input bias current on output shift.

    2. Switch to another Op Amp with CMOS / JFET input structure where the input bias current reduces to the pA range. Let me know if you need help selecting a usable device?

    Additionally, I added a shunt resistor to your 2nd stage (R3) to allow for input bias current flow.

    Regards,

    Hooman

  • Hi,

    Thank you for your helps (I had not seen this bias current). In fact my signal from the hydrophone ( is about 1µV to 300µV). And after your simulation that I modified to have 1µV at the input :

    I think it is impossible to satisfy the maximum variation and the minimum variation. In fact I don't know if I must amplify the signal before before attacking the high pass filter. But what is the minimum voltage level that AOP LT6233 can accept ?

    I think, the better solution is to have a component with with adjustable offset and very low bias current. I don't know if it exists.

    You add a dummy current source : -1.5µA 

         

    But how do we do it electronically ? Is there a dedicated component for this or a specific assembly ?

    But now, I see the problem more clearly thanks to your advice.

    Regards


     

       

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.