Post Go back to editing

Want to use instrumentation amplifier instead of differential amplifier; but it is hard to meet instrumentation amplifier requirement

Hey everyone, 

I am kinda frustrated that I cannot meet the requirement of all the instrumentation amplifier (Analog devices product) that I have bought. 

I have two input signal: 

In+  = DC signal anywhere from 400mV to 700mV 

In- = DC signal anywhere from 100mV to 300mV

Power supply: 9V single supply 

Common Mode Voltage: I do not know. How do you determine that? 

I have used differential amplifier using LTC6800, with a gain of 6, and it works fine.

I want like to use an instrumentation amplifier instead of differential amplifier, and ask you for help. I have tried using diamond plot calculator, and I don't get it. 

Can you please recommend me an instrumentation amplifier?



change titile
[edited by: shurp at 8:07 PM (GMT -4) on 29 Sep 2021]
Parents Reply Children
  • Hmm. I was thinking of using an instrumentation amplifier with the three op-amp configuration but looking at the LTC6800 or LTC2053, they seems different even though it does say that it is an instrumentation amplifier. I guess I will work with this for now. I really wanted to try and use the three op-amp configuration type since there are a lot of those on digikey and mouser.