Post Go back to editing

ADA4945 SE-DIFF conversion simulation

Hi 

I need to convert a ±4.5V single ended signal to a differential signal for an ADC input (probably the LTC2107). Since the input Signal has a -3dB bandwidth of about 50MHz the ADA4945 in high power mode should be sufficient.

The Vocm is set to 1.2V and the gain to 0.267. The Diff-Amp Calculator gives me a decent solution using Rg=280R and Rf=75R. I am using 5V single supply (although a ±5V supply is also possible).

Now when I do simulate the circuit in LTspice the output is not what I would expect: the output should be symmetrical and centered around 1.2V. This is only the case if I do not GND-reference the input voltage source. Also it gets worse at frequencies above 4MHz. See images below.

Questions:

-is this behaviour also to be expected in reality?

-should I use the ADA4930 instead or will it have the same issue (it does show a similar behaviour in the simulation, just starting at higher frequencies)?

-What is the correct way to simulate the SE-DIFF conversion to get around this issue ?

LTspice model with GND referenced input

Transient output at 20MHz ±1V input

AC analysis: outputs with GND referenced input

AC analysis: outputs when removing GND at the input

Parents
  • Hi Damian,

    -is this behaviour also to be expected in reality?

         No, I'm not sure what your whole schematic looks like there. Can you send out your asc file? On my end the transient simulation works fine, similar to the output of the diff-amp calc tool.

    -should I use the ADA4930 instead or will it have the same issue (it does show a similar behaviour in the simulation, just starting at higher frequencies)?
          ADA4945 can do what your intended application is. The problem is the way you have tested it.

    -What is the correct way to simulate the SE-DIFF conversion to get around this issue ?
          In testing the BW of the part your schematic should look like below. The output should be tapped differential and not single ended.

    Regards,
    Goz

Reply
  • Hi Damian,

    -is this behaviour also to be expected in reality?

         No, I'm not sure what your whole schematic looks like there. Can you send out your asc file? On my end the transient simulation works fine, similar to the output of the diff-amp calc tool.

    -should I use the ADA4930 instead or will it have the same issue (it does show a similar behaviour in the simulation, just starting at higher frequencies)?
          ADA4945 can do what your intended application is. The problem is the way you have tested it.

    -What is the correct way to simulate the SE-DIFF conversion to get around this issue ?
          In testing the BW of the part your schematic should look like below. The output should be tapped differential and not single ended.

    Regards,
    Goz

Children