Hi,
I want to use LTC6403-1.
I have a question about the connection with the ADC (AD9253) , so please let me know.
I think the LTC6403-1 is compatible with Zero-I / F.
I would like to connect to the AD9253 with a DC connection. Are there any specific methods or precautions?
・ LTC6403 VOCM = 1.5V
・ AD9253 VIN is rated at 2.0V MAX
⇒ For example, is there a way to convert AD9253 input VCM = 0.9V?
Best Regards,
Naohisa