Post Go back to editing

Questions about ADA4938-1 and ADL5562 for using ADC driver circuit of AD9648

Thread Summary

The user inquired about using two op amps (ADA4938-1 and ADL5562) at the front-end of an AD9648 ADC for additional gain and signal conversion. The support engineer advised that multi-stage input is common for bandwidth and gain requirements, and asked about the operating frequency. The user later clarified that the design concept changed, and they no longer require the additional gain.
AI Generated Content

Hello,

My customer will use AD9648( ADC  )and ADL5562 (ADC driver) in their product.

And they want to add additional amp. (ADA4938-1) for compensating  Gain value at the frond-end of ADL5562.

Q1) Would you advice your opinions about  using 2 op amps at the front-end of AD9648  (Please refer below concept picture.)?

Q2) At the front-end of AD9648 (ADC), is the above concept  usable circuit?

Q3) Can you recommend other components or circuits for this case?

     ( Amp with 5dB Gain + ADL5562 + AD9648)

        1) Need additional 5dB Gain

         2) Change single-ended signal to differential signals

         3) Output signals should be met the input spec. of ADL5562.

 

Regards,

Se-woong

Edit Notes

Correct Typo
[edited by: Se-woong at 4:53 AM (GMT -5) on 1 Dec 2020]