Post Go back to editing

ADCMP370... alternatives

Hi,

We need to use the ADCMP370 to replace a ADCMP371. Unfortunately, there are none in stock anywhere.

The ability of have an open drain that can be pulled up to 15V is of primary importance (most replacements I see are only ~5V tolerant on the output pin which won't work for us)

Is there another, pin to pin compatible part (with the ADCMP370) that can do the same?

Thanks,
Cody

Edit Notes

The reason I am submitting the ticket is that there are none in stock, but didn't say that in original post.
[edited by: CDD_UAA at 11:20 PM (GMT 0) on 15 Jun 2020]

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.