Post Go back to editing

ADA4075 Differential Input Voltage


I want to use ADA4075 for a differential input that could have a maximum of 10V differential voltage.

In the datasheet, I see the absolute maximum rating for Differential Input Voltage is ±1.2 V

What does this mean? The Inputs should have a difference not more than  ±1.2 V? how can I consider it in my design? The inputs are ±5V.

Thanks in advance.



The input could have a maximum of 10V differential voltage.
[edited by: mehran at 7:38 AM (GMT 0) on 29 Apr 2020]