Post Go back to editing

AD8139 Not Working. I need help

Thread Summary

The user is experiencing issues with the AD8139 not outputting any signal on the bench, despite working in SPICE simulations and with the AD8138. The final answer suggests the issue was resolved offline, but recommends converting the circuit to a 4-resistor topology for better performance and less noise. The user noted the input signal amplitude is 0.600V p-p and VCM is 0.36V DC, with supply voltages of ±5V.
AI Generated Content

I am using the AD8139 in the as shown in the attached PDF.

Spice simulations work fine. But On the bench using +-5V supplys,  AD8138 outputs Nothing.

What did I do wrong.

Stan Schekall a783239d66076ba983835f6e0157fe05.pdf

osc_5MHZ.pdf