Post Go back to editing

differential amplifier common mode output

Dear sir,
We are using ADA4927-1 device for our application. In our application input to ADA4927-1 is form a sensor having 
output in Differential mode. we want an output from ADA4927-1 in common mode configuration. we have gone through 
the AN-584 APPLICATION NOTE and we uderstand that we need to give input to PIN No. 2 VOCM form a potential divider.
we request you to give the information  how to take output from ADA4927-1 in common mode ( ie What to do for one of the unused 
pin No. 10 or 11 of ADA4927-1) and potential divider voltage to be  given to Pin. No. 2 of the Ada4927-1 for getting the common mode output.

please do the needful to me....


Parents
  • You can compensate for the offset (and retain the dc component of your signal) with the circuit shown at the end of this email.

    Need the same RCM in both sides to retain balance. One RCM is usually grounded the other is connected to a reference voltage that will cancel input dc offset as well as the input offset of the diff-amp.

    The value of RCM is large compared to Rg.

    For Fixed compensation VREF can be VCC or VEE. In this case, you determine the input side that is at higher dc level and connect that RCM to ground. Apply a VREF to cancel out all nominal offsets.

    For dynamic compensation, VREF can come from a DAC. In this case the value of VREF is controlled dynamically. The dc offset is measured in the digital domain at some appropriate instant ( for example at power up) when the inputs are at a known “zero” state and a correction code is input to a DAC whose output is VREF.

    The accuracy of this correction can be made quite high if the value of RCM is high.

    Message was edited by: AndyR Removed Email Footer Information

Reply
  • You can compensate for the offset (and retain the dc component of your signal) with the circuit shown at the end of this email.

    Need the same RCM in both sides to retain balance. One RCM is usually grounded the other is connected to a reference voltage that will cancel input dc offset as well as the input offset of the diff-amp.

    The value of RCM is large compared to Rg.

    For Fixed compensation VREF can be VCC or VEE. In this case, you determine the input side that is at higher dc level and connect that RCM to ground. Apply a VREF to cancel out all nominal offsets.

    For dynamic compensation, VREF can come from a DAC. In this case the value of VREF is controlled dynamically. The dc offset is measured in the digital domain at some appropriate instant ( for example at power up) when the inputs are at a known “zero” state and a correction code is input to a DAC whose output is VREF.

    The accuracy of this correction can be made quite high if the value of RCM is high.

    Message was edited by: AndyR Removed Email Footer Information

Children
No Data