Post Go back to editing

differential amplifier common mode output

Dear sir,
We are using ADA4927-1 device for our application. In our application input to ADA4927-1 is form a sensor having 
output in Differential mode. we want an output from ADA4927-1 in common mode configuration. we have gone through 
the AN-584 APPLICATION NOTE and we uderstand that we need to give input to PIN No. 2 VOCM form a potential divider.
we request you to give the information  how to take output from ADA4927-1 in common mode ( ie What to do for one of the unused 
pin No. 10 or 11 of ADA4927-1) and potential divider voltage to be  given to Pin. No. 2 of the Ada4927-1 for getting the common mode output.

please do the needful to me....


Parents
  • HI Gustavo,

    I am using differential amplifier ADA4927 to drive ADC. Differential input given to the amplifer is having 10mV differential dc offset, i.e. differential input is riding on 5mV differential dc. How can I cancel this DC offset in the output? Output of the amplifier has to be DC coupled to ADC. Suggest appropriate circuit.

    Thanks and Regards,

    Dwijen

Reply
  • HI Gustavo,

    I am using differential amplifier ADA4927 to drive ADC. Differential input given to the amplifer is having 10mV differential dc offset, i.e. differential input is riding on 5mV differential dc. How can I cancel this DC offset in the output? Output of the amplifier has to be DC coupled to ADC. Suggest appropriate circuit.

    Thanks and Regards,

    Dwijen

Children
No Data